cancel
Showing results for 
Search instead for 
Did you mean: 

Reading the H7 temperature sensor calibration parameters

Peter Mather
Associate III
Posted on June 28, 2018 at 18:34

STM32H743

To improve the accuracy of the temperature sensor measurement, each device is individually factory-calibrated by ST. The temperature sensor factory calibration data are stored by ST in the System memory area, which is accessible in Read-only mode

Please could someone point me at where I can find information on how to read the calibration parameters. Can't see anything in the device manual, the H7 reference manual or the HAL manual but probably missed it.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud GARSI
ST Employee
Posted on June 28, 2018 at 19:04

Hello Peter,

Please refer to the

https://www.st.com/resource/en/datasheet/stm32h743bi.pdf

 .

The memory addresses for temperature sensor raw data acquired values, at VDDA= 3.3V , 30°C and 110°C , are provided in table 90 ' Temperature sensor calibration values'.

Khouloud.

View solution in original post

4 REPLIES 4
john doe
Lead
Posted on June 28, 2018 at 18:57

You dont mention which chip you're using but check section 6 of your data sheet for a table 'Temperature sensor calibration values' and it shows the register location and values

Khouloud GARSI
ST Employee
Posted on June 28, 2018 at 19:04

Hello Peter,

Please refer to the

https://www.st.com/resource/en/datasheet/stm32h743bi.pdf

 .

The memory addresses for temperature sensor raw data acquired values, at VDDA= 3.3V , 30°C and 110°C , are provided in table 90 ' Temperature sensor calibration values'.

Khouloud.

Peter Mather
Associate III
Posted on June 29, 2018 at 12:22

Thanks - the manuals are so large that sometimes you have to know where to look.

one V
Associate III

The data I read is TS_CAL1:12309, TS_CAL2:15501. Temprature: 80*(HAL_ADC_GetValue(&hadc3)* 3.300f / 4096 - getTS_CAL1()) / (getTS_CAL2() - getTS_CAL1()) + 30, is it right? Is your problem solved? Can you give me the code to give me a reference?