2023-03-06 6:45 AM
I have a custom board with STM32H725IG using a multiplexed Octo SPI memory S71KL256xx. I have managed to establish reasonable communication to the memory thanks to example given in AN5050 even tough it was not H7. Sometimes, however, there are read/write errors and I suspect my PCB is poor. A new PCB will come soon.
In the meanwhile, I am struggling writing a custom external loader. I have used the H7-example from stm32-external-loader/Loader_Files at contrib · STMicroelectronics/stm32-external-loader (github.com).
I am using the same linker script given from the link, but in the Init() function in Loader_Src.c, the MX_OCTOSPI1_Init() hangs...
int Init()
{
// Inits taken from Github example
// https://github.com/STMicroelectronics/stm32-external-loader/blob/contrib/Loader_Files/H7%20device/Loader_Src.c
*(uint32_t*)0xE000EDF0 = 0xA05F0000; //enable interrupts in debug
SystemInit(); // called in system_stmh7xx.c
/* ADAPTATION TO THE DEVICE
* change VTOR setting for H7 device
* SCB->VTOR = 0x24000000 | 0x200;
*
* change VTOR setting for other devices
* SCB->VTOR = 0x20000000 | 0x200;
* */
SCB->VTOR = 0x24000000 | 0x200;
__set_PRIMASK(0); //enable interrupts
// System inits moved from main.c
HAL_Init();
SystemClock_Config();
PeriphCommonClock_Config();
MX_GPIO_Init();
// Reset peripheral
// Taken from Githug link as above and
// modified from QUAD SPI to OCTO SPI
__HAL_RCC_OSPI1_FORCE_RESET();
__HAL_RCC_OSPI1_RELEASE_RESET();
__HAL_RCC_OSPI2_FORCE_RESET();
__HAL_RCC_OSPI2_RELEASE_RESET();
// HANGS HERE...
MX_OCTOSPI1_Init();
MX_OCTOSPI2_Init();
// Set up memory mapped configuration for
// multiplexed OCTO SPI SLK256SC0BHB000
EnableMemMapped();
__set_PRIMASK(1); //disable interrupts
return 1;
}Setting breakpoints, it hangs more specificly when HAL_OSPI_HyperbusCfg is called below:
sHyperBusCfg.RWRecoveryTime = 3;
sHyperBusCfg.AccessTime = 6;
sHyperBusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;
sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
if (HAL_OSPI_HyperbusCfg(&hospi1, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}Setting further breakpoints in the HAL_OSPI_HyperbusCfg() the fault occurs in the first if-statement below which is false:
if ((state == HAL_OSPI_STATE_HYPERBUS_INIT) || (state == HAL_OSPI_STATE_READY))
{
/* Wait till busy flag is reset */
status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_BUSY, RESET, tickstart, Timeout);
if (status == HAL_OK)
{
/* Configure Hyperbus configuration Latency register */
WRITE_REG(hospi->Instance->HLCR, ((cfg->RWRecoveryTime << OCTOSPI_HLCR_TRWR_Pos) |
(cfg->AccessTime << OCTOSPI_HLCR_TACC_Pos) |
cfg->WriteZeroLatency | cfg->LatencyMode));
/* Update the state */
hospi->State = HAL_OSPI_STATE_READY;
}
}
else
{
status = HAL_ERROR;
hospi->ErrorCode = HAL_OSPI_ERROR_INVALID_SEQUENCE;
}
/* Return function status */
return status;Please, any ideas what could be wrong here..?
Thanks in advance
Solved! Go to Solution.
2023-03-17 5:40 AM
Clearing memory states prior to the OCTOSPI- configuration made the trick:
hospi1.State = 0;
hospi2.State = 0;
MX_OCTOSPI1_Init();
MX_OCTOSPI2_Init();
2023-03-17 5:40 AM
Clearing memory states prior to the OCTOSPI- configuration made the trick:
hospi1.State = 0;
hospi2.State = 0;
MX_OCTOSPI1_Init();
MX_OCTOSPI2_Init();