cancel
Showing results for 
Search instead for 
Did you mean: 

TSDHD STM32H7S7I8T6

Y007
Associate

 

Hello ST Community,

I am using TSD HD Gen4-STM32-43CT-01 display module which has STM32H7S7I8T6 MCU.
I am facing an issue where I am unable to connect or disconnect the debugger using MB1440C, while the same debugger works perfectly with other TSD HD Gen4 displays.

Debugger setup

  • Debugger: MB1440C

  • Interface: SWD

  • Connections:

    • SWDIO → JTMS

    • SWCLK → JCLK

    • GND → GND

This setup was working earlier on the same board.

What changed

The last firmware flashed was a boot-level application intended to write custom data into external QSPI flash:

  • External Flash: GD25Q127CS (128 Mbit)

After flashing this boot code:

  • The MCU is no longer connectable via SWD

  • ST-LINK / MB1440C cannot attach

  • Power cycling does not help

Observations

  • Same MB1440C debugger + same CubeIDE works fine with other TSD HD displays

  • Issue is specific to this board after boot code flashing

  • I suspect:

    • SWD pins may be reconfigured as GPIO

    • Option Bytes may have been modified

    • Boot code may be disabling debug or putting MCU in low-power/reset loop

    • External QSPI initialization may be locking the system early

I would appreciate any guidance on hardware recovery steps, forced boot modes, or debugger connection techniques specific to STM32H7S7.

Thank you in advance.






1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Maybe you have mistakenly activate one of a security feature in the target MCU.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

Maybe you have mistakenly activate one of a security feature in the target MCU.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello,
Thank You,
So How should I debug that or Erase the Flash?