cancel
Showing results for 
Search instead for 
Did you mean: 

problem to install st-link driver

Sanand97
Associate II

Hi!

I have a board nucleo F446RE..

I can't to install the st-link driver.

can be related to fact that in my laptop I have windows 11?

 

11 REPLIES 11
Pavel A.
Super User

ST-Link driver (a modern one)  has no problems with Win11.

Ok, thanks!

Sorry, but I'm new..

Is important to install other STM softwares before to install the st-link driver?

No, the ST-LINK driver depends only on the Windows in-box winusb feature. But the debuggers and programming software for STM32s certainly have more dependencies.

 

TDK
Super User

Perhaps you can share more about why you're unable to install the driver so that the replies can be more focused and useful. What happens when you try? What error message or unexpected behavior do you get? Show screenshots if possible.

If you feel a post has answered your question, please click "Accept as Solution".

So, I have downloaded the en.stsw-link009 and I have launched dpinst_amd64.exe, with the board connected, but I receive this window.

Sanand97_0-1720821420913.png

 

Therefore?

Best guess is some antivirus software or "protection" software is preventing driver installation.

Can STM32CubeProgrammer install successfully? And can it connect to the board? It should install drivers as well.

If you feel a post has answered your question, please click "Accept as Solution".

I can't to install stm 32cube programmer because I'm not the pc-administrator.. 

Maybe this is the problem

Pavel A.
Super User

Yes maybe installing drivers failed because it could not elevate.

Please look in c:\windows\dpinst.log  and \windows\INF\setupapi.dev*.log (most recent files)