cancel
Showing results for 
Search instead for 
Did you mean: 

Power Profiling Tool for STM32 Applications

darla14
Senior
Posted on August 02, 2016 at 06:52

In the STM32CubeMX there is Power Consumption Calculator Tool.But this is for new code to be developed.

Is there any other tool or this tool available for the already developed Application?

There is tool for TI's MSPs  like this -> 

http://www.ti.com/tool/energytrace

Wish to get the similar tool for ST's MCU as well.

Also how much the parameters from this tool will vary as compared to the actual measurements done by the meters?(%age wise , 

�10-15??)

Thanks in advance !

Regards,

Rp

#!stm32 #powerconsumption
2 REPLIES 2
Nesrine M_O
Lead II
Posted on August 02, 2016 at 11:32

Hi Rp,

The power consumption calculator (PCC) in STM32CubeMX returns average of current consumption, Battery life… these data are taken from the MCU datasheet or interpolated from a user specified bus or core frequency.

And this tool is for applications developed with CUBEMX.

Refer to the Power Consumption Calculator (PCC) view section in the UM1718 User manual for more details.

I will forward you suggestion about the tool to our CUBEMX team.

-Syrine-

Imen.D
ST Employee
Posted on January 09, 2018 at 17:53

Hi,

The

should answer you request.
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen