cancel
Showing results for 
Search instead for 
Did you mean: 

Power consumption of STM32L412XX

akhilfrancis
Associate

Hi, I am doing a comparison between the STM32L432 and the STM32L412. However, I observed a discrepancy in the STM32L412 power values under Table 4. STM32L412xx modes overview, LPRun and LPSleep are showing the same value. Is this correct? 

akhilfrancis_0-1742620945851.png

 

4 REPLIES 4
KnarfB
Principal III

Looks like an error in DS12469 Rev 9 data sheet. Would expect a value slightly below STM32L432xx (DS11451 Rev 4). Sleep is a feature of the Arm Cortex-M4 core.

hth

KnarfB

Could you please confirm if this error is officially acknowledged and if there is an errata or updated documentation addressing the discrepancy? If not, may I assume that it's simply incorrect data in the datasheet?

KDJEM.1
ST Employee

Hello @akhilfrancis and welcome to the community;

 

Thank you for bringing this issue to our attention.

I reported internally for checking.

Internal ticket number: 205937 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hello @akhilfrancis;

 

I confirm that this is a typo and will be corrected in the coming version of the datasheet.

Please use detailed "Table 40. Current consumption in Sleep and Low-power sleep modes, flash ON" and "Table 42. Current consumption in Low-power sleep modes, flash in power-down" in DS12469 for LPSleep current consumption.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.