cancel
Showing results for 
Search instead for 
Did you mean: 

Power consumption issue with STM32L073VBT6.

ren yong
Associate II
Posted on October 28, 2017 at 12:45

 I have my own product board with STM32L073VBT6.The power comsumption increase to 10mA (an other is 4mA) when enter low power mode.So I had removed all other chips only left the STM32 and found out that the MCU cost the 10mA. The function of the chip is ok. I Don't understand How the chip came to that with the function ok.

?????STM32L073??pCB????????10mA??????????????IC??????????3?mA????????????????????????

#stm32l073 #low-power-run #issue
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on October 28, 2017 at 16:47

Unfortunately your post lacks sufficient detail to replicate or understand the circuit and software as implemented.

Is this with a debugger attached?

How to you make a determination about the internal state of the processor?

Sleep/Standby?

External buffers, LEDs, pull up/down resistors?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ren yong
Associate II
Posted on November 08, 2017 at 02:27

         Just power on with 3.3 the mcu,and connect the reset pin to gnd.