cancel
Showing results for 
Search instead for 
Did you mean: 

power consumption by STM32H735VGH on full speed ADC configuration

shaktipg
Associate II

The total power consumption by STM32H735VGH at full speed interleaved mode differential adc configuration?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

The datasheet has details about power consumption of various peripherals. It will depend on more information than you're providing, such as what other peripherals are active, what the clock speed is, cache settings, etc.

Generally, the processor will use tens to hundreds of mA and the clock speed has the biggest correlation to power draw. Low-power modes are also a possibility.

Here is one of many such power consumption tables from the datasheet:

TDK_0-1698415819965.png

And the datasheet:

https://www.st.com/resource/en/datasheet/stm32h735ag.pdf

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Guru

The datasheet has details about power consumption of various peripherals. It will depend on more information than you're providing, such as what other peripherals are active, what the clock speed is, cache settings, etc.

Generally, the processor will use tens to hundreds of mA and the clock speed has the biggest correlation to power draw. Low-power modes are also a possibility.

Here is one of many such power consumption tables from the datasheet:

TDK_0-1698415819965.png

And the datasheet:

https://www.st.com/resource/en/datasheet/stm32h735ag.pdf

If you feel a post has answered your question, please click "Accept as Solution".