cancel
Showing results for 
Search instead for 
Did you mean: 

Please confirm PB12 pin location for STM32F469xx

Tai.Cheng Chung
Associate II
Posted on February 25, 2016 at 03:23

Hi:

  Can STM guys help to make sure the PB12 location @ LQFP176 of STM32f469xx. On datasheet (DM00219980) Figure 1 (@page 14). pin 85 is mark as  PH8. However  @ Table 10 (@page59) pin 85 is PB12. Which is correct?
3 REPLIES 3
Nesrine M_O
Lead II
Posted on February 26, 2016 at 11:36

Hi Calvin63,

Table 10 is correct .

Figure 1 and 16, are already planned to be updated in next version.

-Syrine-

Tai.Cheng Chung
Associate II
Posted on March 01, 2016 at 01:43

Hi Syrine:

   Thank you. The DM00172465 (AN4675) use the same table and should be updated also.

Nesrine M_O
Lead II
Posted on March 01, 2016 at 15:21

Hi Calvin63,

Thanks for highlighting the issue.it will be updated in next version.

-Syrine-