2022-09-07 03:01 AM
Please advise what is the suffix "SP2" in the type 32F45VGT6? Please confirm if this mean device is already programmed?
Solved! Go to Solution.
2022-09-07 03:09 AM
No, it is not a programmed component, but the specification with the $P2 at the end (32F745VGT6$P2) is an internal marking. Relevant for the application is the first line, here STM32F745VGT6.
Regards
/Peter
2022-09-07 03:09 AM
No, it is not a programmed component, but the specification with the $P2 at the end (32F745VGT6$P2) is an internal marking. Relevant for the application is the first line, here STM32F745VGT6.
Regards
/Peter
2022-09-07 04:51 AM
thank you so much for the quick response.
2022-09-07 04:53 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter