cancel
Showing results for 
Search instead for 
Did you mean: 

Pinout and Configuration functions disabled?

willgordge
Associate

Trying to configure my project to use USART2. When I opened "System Core" and "Connectivity", I see that a bunch of options are disabled or have warning signs. I haven't been able to find out why or how to change them, and this isn't an issue I have run into before... so any help would be greatly appreciated!

Screenshot 2024-03-10 at 16.39.36.png

 

1 REPLY 1
STTwo-32
ST Employee

Hello @willgordge and welcome to the ST Community 😊.

Those signs means that you can't use this peripheral (for the red cirecle sign) or maybe some of this peripheral configurations are not possible (for the yellow triangle). For example if you are using all SPI5 available pins for other functions, you can't use this SPI interface.

I suggest you to put the Cursor on the IP name. A message will appear to explain why this not possible to use. 

here is two examples:

STTwo32_0-1710140766063.png

STTwo32_1-1710140851797.png

 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.