2019-06-25 03:02 AM
I try the STM32demo /PIL/Test_PIL_IIR_Filter with the matlab 2018,
###Startup file:
###Startup path:
### Start compile .c source IIR_Filter_int32.c
### Successfully compiled source IIR_Filter_int32.c
### Start compile .c source main.c
### Successfully compiled source main.c
"### BUILD_MODE model_reference"
"### Generated IIR_Filter_int32_rtwlib.lib model_reference"
"### Created IIR_Filter_int32_rtwlib.lib successfully (or it was already up to date)"
### Real-Time Workshop build procedure for method: 'after_make
### modelName: 'IIR_Filter_int32
### gcs: 'IIR_Filter_int32
### bdroot: 'IIR_Filter_int32
### Real-Time Workshop build procedure for method: 'exit
### modelName: 'IIR_Filter_int32
### gcs: 'IIR_Filter_int32
### bdroot: 'IIR_Filter_int32
### Successful completion of Real-Time Workshop build procedure for model: IIR_Filter_int32
### Connectivity configuration for referenced model "IIR_Filter_int32": STM32 PIL ###
Error:An error occurred while creating an instance of connectivity configuration class "stm32Pil.ConnectivityConfig". Check that this is a valid connectivity configuration class.
Caused by:
组 STM32 中�?存在首选项 STM32FileName
2019-08-20 02:35 AM
Hi @Kg ,
This problem is not reproduced with the version 5.1.0 of STM32-MAT/TARGET, published end of July 2019.
While working on this version the followings tests were successful for PIL:
- F429ZITx @ 180 Mhz, USART1: OK
- L476RG @ 80 Mhz, USART2: OK
Regards.
Cyril