2017-05-02 12:49 PM
I have made a board on which I plug the Nucleo-F767ZI microcontroller board. There is one GPIO pin that I cannot get to function as a digital output: PG2.
This is my code in mbed-os:
static
DigitalOut
myPin_A
(PG_2
);static
DigitalOut
myPin_B
(PG_3
);...
static
void
someFunction
(){
myPin_A
.write
(1);// <- This one doesn't work :(
myPin_B
.write
(1);// <- But this one works!
}
I thought: 'Perhaps this problem has to do with mbed-os'. So I have tried the ST HAL:static
void
someFunction
()
{
GPIO_InitTypeDef
GPIO_InitStruct
;
GPIO_InitStruct
.Pin =
GPIO_PIN_2
;GPIO_InitStruct
.Mode =
GPIO_MODE_OUTPUT_PP
;GPIO_InitStruct
.Pull =
GPIO_NOPULL
;GPIO_InitStruct
.Speed =
GPIO_SPEED_FREQ_LOW
;HAL_GPIO_Init
(
GPIOG
, &GPIO_InitStruct
);GPIO_InitStruct
.Pin =
GPIO_PIN_3
;GPIO_InitStruct
.Mode =
GPIO_MODE_OUTPUT_PP
;GPIO_InitStruct
.Pull =
GPIO_NOPULL
;GPIO_InitStruct
.Speed =
GPIO_SPEED_FREQ_LOW
;HAL_GPIO_Init
(
GPIOG
, &GPIO_InitStruct
);HAL_GPIO_WritePin
(GPIOG
,GPIO_PIN_2
,GPIO_PIN_SET
);// <- This one doesn't work :(
HAL_GPIO_WritePin
(GPIOG
,GPIO_PIN_3
,GPIO_PIN_SET
);// <- But this one works!
}
As you can see, I get exactly the same result. I've tried another Nucleo-F767ZI board standalone - I don't plug it into my custom board to reassure myself that the PG2 pin isn't affected by anything outside the Nucleo - but still got the same result.
I have posted my question also on StackOverflow:
EDIT
I have generated a new project from scratch with CubeMX. As you know, CubeMX does not support mbed-os, but freeRTOS instead. When using freeRTOS, the pin
PG_2
works, using the code given above.
Why don't I get it working when mbed-os is running? This is so strange :(
#stm32f767zi-nucleo #stm32f767zi-nucleo-board #mbed #stm32f7672017-05-02 2:57 PM
Check the GPIOG registers in debugger. You can also wiggle the pin there through ODR and/or observe its state in IDR.
JW