cancel
Showing results for 
Search instead for 
Did you mean: 

PDR_ON Floating

shubhenduatadben
Associate III

Dear,

    We are working on a custom design which has PDR_ON pin floating. The board is already fabricated and assembled.

    The part number is STM32H7A3AII6Q.

    Please let us know if this has any consequences on normal operation of the MCU and if so, what's the wayout.

Regards-

Shubhendu

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

PDR_ON pin needs to be pulled up to VDD or pulled down to the VSS.

Since you forgot to do that, you may face instability especially on the reset behavior when the power is low and also instability on the VBAT usage:

AN5307:

SofLit_0-1738149505977.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

PDR_ON pin needs to be pulled up to VDD or pulled down to the VSS.

Since you forgot to do that, you may face instability especially on the reset behavior when the power is low and also instability on the VBAT usage:

AN5307:

SofLit_0-1738149505977.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.