2022-11-27 12:41 AM
I would like to test STM32F4/L4/H7 based boards with emulated testing software on a PC.
I need to test all standard serial communication protocols along with injecting external PPS or interrupt.
I need an PCI or USB adaptors or cards, and a software API / PC drivers in order to do that VIA PC.
Any suggestions?
2022-11-27 4:55 AM
Get another STM32 board, connected to a PC via UART or USB or whatever.
Run the "host" side on it. No adapters, drivers, no headache.
2022-11-27 6:58 AM
+1
You can use DISCO or NUCLEO boards to generate test patterns, pin or peripheral IO.
The board could have a GPS/GNSS to generate timing, if that's critical.
Use a serial protocol to drive the test sequences, or download vectors, etc.
Connect via COM/TTY, host side software can then be built with languages/tools of your choice.
Having buffering to protect the board. Consider a routing/mother board to host the card, and connect with wiring harnesses or pogo pins, etc.
Alternatives probably LabView or Advantech
2022-11-27 11:55 AM
What is your opinion about these interface cards?
It can be used with LabView or with our own application.
Thanks.