2019-10-09 1:39 AM
Hi,
I'm trying to send data from STM32F767Zi to another node using CANBUS protocol....it starts sending data every second and at other node i can get data, but all of a sudden data stops transmitting,when i debug i finding HAL_CAN_ERROR_PARAM.
what could cause the error and how do i resolve it!!
Thanks,
Vimal
2019-10-11 6:53 AM
Hello,
Did you generate a STM32CubeMx project ?
I suggest you to inspire from the CAN examples under the STM32F7 cube firmware package: STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I_EVAL\Examples\CAN
This may helps you on your application.
Best Regards,
Imen
2019-10-14 8:13 AM
Yes i have used the one which was in the firmware package.In that sometimes i'm getting that above error.
Please let me know how to solve this.
Thanks
Vimal
2019-10-14 8:23 AM
Seen a couple of reports of this, you'll have to debug into the HAL library code to understand what fields/parameters it is objecting too, or what peripheral state is causing this to flag.