cancel
Showing results for 
Search instead for 
Did you mean: 

output of DAC to input of ADC

nemisha
Associate II
Posted on July 16, 2015 at 15:52

Good Afternoon Everyone,

 Is it possible that on STM32F4 , I first do a DAC and then use its output as input to ADC and finally get a digital output ?

If I can do that , how can I do this connection in between the DAC o/p and ADC  i/p ?

Sorry if the question is invalid. Thank you all in advance.

Regards

#discovery #stm32f4 #stm32f4-adc
1 REPLY 1
Posted on July 16, 2015 at 16:24

I haven't tried it, but I suspect it would probably work, provided the DAC pin has enough drive.

.. and finally get a digital output

Not really sure what that means, the ADC can provide a 12-bit value, and you could print that out, I guess.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..