2022-09-14 07:45 PM
2022-09-14 09:13 PM
Perhaps one of the engineers responsible for the design can help you?
Does behaviour change if BOOT0 is pulled high?
2022-09-14 11:22 PM
Not detected where ? SWD USB USART ....
Is MCU in STOP or STANDBY ? Use under reset connect mode if SWD...
2022-09-15 09:58 PM
I tried to program using ST link and Cube IDE. Sharing the screenshot here.
2022-09-15 10:13 PM
2022-09-15 10:52 PM
NO.will get an error "NO STM 32 target found ! " is the erroe message we get
2022-09-15 10:52 PM
I Changed but still the condition is same.
2022-09-15 11:13 PM