cancel
Showing results for 
Search instead for 
Did you mean: 

OCTOSPI on STM32U5F9ZJT6Q

Ivica
Associate

Dear, 

Can you confirm that OCTOSPI P2 is available only on WLCSP208 and TFBGA216 packages of this series? 

I wanted to use both OCTOSPI interfaces in LQFP144, but noticed that there is missing only OCTOSPIM_P2_IO3 line in it, so my conclusion is that LQFP144 supports only one OCTOSPI. Is that right? 

Thank you. 

5 REPLIES 5
KDJEM.1
ST Employee

Hello @Ivica,

 

According to the datasheet DS14395 Rev 2 Table 2. STM32U5Fxxx features and peripheral counts.

The STM32U5F9ZJ supports only one OCTOSPI interface. If you want to use two XSPIs interfaces with STM32U5F9ZJ package, I recommend you to use the OCTOSPI interface and HSPI interface, which are supported on STM32U5F9ZJ package.

KDJEM1_0-1736346535539.png

KDJEM1_1-1736346286456.png

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Is there a way to mux/map via the SPIM provided one can escape OCTOSPIM_P2_NCS on exposed pins?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you @KDJEM.1 I missed this table. Then it is clear regarding OCTOSPI. 

Hello @Tesla DeLorean

 

Thank you for bringing this to our attention.

I will check internally is there any restriction to use the multiplexed mode on STM32U5F9ZJ? And there a way to mux/map via the SPIM provided to escape OCTOSPIM_P2_NCS?

Internal ticket number: 199853 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

 

I confirm that the STM32U5F9ZJ supports the multiplexed mode.

This behavior will be explained in the coming datasheet revision, for example by adding note for STM32U5F9ZJ package “Two OCTOSPIs are available only in muxed MODE “ on table 2

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.