cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLO-H755ZI-Q Unable to debug CM4

Vero
Associate II

Hi community,

I build and program both CM without error and debugger configuration as in the AN5361 .

The Nucleo- runs with maximum frequency  480 MHz, and Power supply:

  HAL_PWREx_ConfigSupply(PWR_SMPS_2V5_SUPPLIES_LDO);

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

 

 I am debugging the CM7 however I'm not able to debug CM4 and have this error :

 

Starting server with the following options:

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

 

Failed to read ROM table via AP 3

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.

 

I've already tried with the advice of:

Unable to connect to STM32H7 devices - STMicroelectronics Community

 

can you help me?

1 ACCEPTED SOLUTION

Accepted Solutions

The power mode is used for synchronization between CM7 and CM4.

These lines in main.c (CM4) are used for low power mode

  HAL_PWREx_ClearPendingEvent();
  HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D2_DOMAIN);

Uncomment these two lines but you will lose the synchronization between the cores. Here, CM7 needs to start before  CM4 to configure the system before to release CM4 and wake it up from stop mode.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello,

Did you modify your board HW to get SMS/LDO power config?

Also, if the CM4 is using Low power mode the debug will be lost.

Also becareful : @480MHz you need to set VOLTAGE_SCALE0.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks. 

If I would likes to use only the SMS I can modified:

HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY)

but I don't see this option for the  NUCLO-H755ZI-Q on the cube menu. can I set it manually?

In this case the hw changes will not be needed... correct?

Where can I check on Cube the low Power mode of M4?

Them i will put the VOLTAGE_SCALE0.

SofLit
ST Employee

The NUCLO-H755ZI-Q board is in SMPS configuration.

The power configuration can be set in RCC menu:

SofLit_0-1712597769131.png

Attached an example of .ioc file for this board.

Warning 1: in SMPS mode you cannot exceed a system frequency of 400MHz/VOS1.

You need to set VOLTAGE_SCALE1 in this configuration.

According to the datasheet:

SofLit_1-1712598020082.png

Warning 2: the software power configuration you load to the MCU should reflect the HW power configuration of your board, otherwise the MCU will be temporarily "lost" and you need to recover the chip by a specific manipulation.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

The power mode is used for synchronization between CM7 and CM4.

These lines in main.c (CM4) are used for low power mode

  HAL_PWREx_ClearPendingEvent();
  HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D2_DOMAIN);

Uncomment these two lines but you will lose the synchronization between the cores. Here, CM7 needs to start before  CM4 to configure the system before to release CM4 and wake it up from stop mode.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.