2023-03-07 01:39 AM
Init-Sequnece:
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.GainCompensation = 0;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc1.Init.OversamplingMode = ENABLE;
//hadc1.Init.OversamplingMode = DISABLE;
hadc1.Init.Oversampling.Ratio = ADC_OVERSAMPLING_RATIO_2;
hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_1;
hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_RESUMED_MODE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
with 'hadc1.Init.OversamplingMode = DISABLE;' everything works as expected ..
2023-03-07 05:46 AM
solution found:
this is bug in parameter defines in oversampling. Please find reported bug in Github will be fixed in next release.
https://github.com/STMicroelectronics/STM32CubeU5/issues/18
ADC1 oversampler is specific and there is no sampling ration step like 2,4,8,16....
But it's smoother 0,1,2,3,...
as a hot fix you can use direct access register
//SET_BIT(ADC1->CFGR2, ADC_CFGR2_ROVSE);
MODIFY_REG(ADC1->CFGR2, ADC_CFGR2_OVSR_Msk, ADC_CFGR2_OVSR_0); //Ratio 2
MODIFY_REG(ADC1->CFGR2, ADC_CFGR2_OVSR_Msk, ADC_CFGR2_OVSR_1|ADC_CFGR2_OVSR_0); //Ratio 4
2023-03-07 09:44 PM
Can you provide the whole solution. And explain more?