2021-07-02 1:29 AM
I am using NUCLEO-L4R5ZI-P board, I have measured current consumption by using example project (PWR Mode: STOP1) and I got the following readings :
Practically STOP1 : 1.19 uA
Datasheet STOP1 : 4 uA
Why I am not getting same value mentioned in datasheet is there something wrong?
Solved! Go to Solution.
2021-07-02 3:56 AM
Hello @Brajp.1,
When checking the STM32L4R5ZI datasheet, the Current consumption in Stop 1 mode is represented in the following table:
Can you precise which datasheet you are working with and the mode you are using?
Chahinez.
2021-07-02 3:56 AM
Hello @Brajp.1,
When checking the STM32L4R5ZI datasheet, the Current consumption in Stop 1 mode is represented in the following table:
Can you precise which datasheet you are working with and the mode you are using?
Chahinez.
2021-07-02 4:10 AM
I am using following datasheet:
I am using STOP1 mode.
2021-07-02 4:18 AM
2021-07-02 5:15 AM
Hi,
The table of the application note you are referring to concerns the L4 product while you are working with the L4+, please check the note I highlighted in the screenshot below:
To check the correct values of the power consumption I advise you to refer to the datasheet of STM32L4R5xx since it contains different use cases presented in the table 46.
Chahinez,