cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-L4R5ZI-P STOP1 mode current consumption is not matching datasheet

Brajp.1
Associate II

I am using NUCLEO-L4R5ZI-P board, I have measured current consumption by using example project (PWR Mode: STOP1) and I got the following readings :

Practically STOP1 : 1.19 uA

Datasheet STOP1 : 4 uA

Why I am not getting same value mentioned in datasheet is there something wrong?

1 ACCEPTED SOLUTION

Accepted Solutions
ChahinezC
Lead

Hello @Brajp.1​,

When checking the STM32L4R5ZI datasheet, the Current consumption in Stop 1 mode is represented in the following table:

0693W00000BcfFvQAJ.png 

Can you precise which datasheet you are working with and the mode you are using?

Chahinez.

View solution in original post

4 REPLIES 4
ChahinezC
Lead

Hello @Brajp.1​,

When checking the STM32L4R5ZI datasheet, the Current consumption in Stop 1 mode is represented in the following table:

0693W00000BcfFvQAJ.png 

Can you precise which datasheet you are working with and the mode you are using?

Chahinez.

0693W00000BcfOiQAJ.png

ChahinezC
Lead

Hi,

The table of the application note you are referring to concerns the L4 product while you are working with the L4+, please check the note I highlighted in the screenshot below:

0693W00000Bcfk0QAB.png 

To check the correct values of the power consumption I advise you to refer to the datasheet of STM32L4R5xx since it contains different use cases presented in the table 46.

Chahinez,