2018-04-06 4:04 AM
Hi Team,
I have issue in debugging NUCLEO-L4R5ZI, i m facing with following error, for the IOToggle code.
Please let me know what i need to change in the below script. to fix the issue to proceed in debug.
IDE: Atollic IDE.
♯ Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2/F4 microcontrollers
♯ Uncomment next line, 2=32 bit, 1=16 bit and 0=8 bit parallelism mode&sharpmonitor flash set_parallelism_mode 2♯ Set character encoding
set host-charset CP1252set target-charset CP1252♯ Reset to known state
monitor reset♯ Load the program executable
load♯ Reset the chip to get to a known state. Remove ''monitor reset'' command
♯ if the code is not located at default address and does not run by reset. monitor reset♯ Enable Debug connection in low power modes (DBGMCU->CR)
set *0xE0042004 = (*0xE0042004) | 0x7♯ Set a breakpoint at main().tbreak main♯ Run to the breakpoint.
continueRegards,
Phanirajkiran
#debug-issue2018-04-08 11:13 PM
HI Team,
Im facing issue with NUCLEO-L4R5ZI, startup script.
When i try to debug the board/ program board. It throws me a error.
2018-04-09 2:21 AM
Solution: