STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Having trouble getting an STM32L433 working as an I2C slave

So I have written some code and gotten it partially to work. But after running for a few seconds with an I2C master sending requests and the STM32L433 responding, it receives an address match for the slave to receive and then the receive is terminate...

DPaxs by Associate
  • 829 Views
  • 1 replies
  • 0 kudos

STM32F091RCTx SPI send issue

I'm using STM32CubeMX v4.25.0 to generate the HAL files for SPI2 and Attolic TrueSTUDIO to compile/debug my application. My intent is to communicate with external flash. Sending/receiving commands with "HAL_SPI_TransmitReceive_IT", everything works f...

LSant by Associate
  • 765 Views
  • 1 replies
  • 0 kudos

Problem with ADC and DMA

Posted on July 13, 2018 at 22:03Hello community! I've got a problem with DMA and ADC (multi channel). I can't find solution why function HAL_ADC_Start_DMA returns 0's to the 'adc_value' array. I have connected to Nucleo F466RE board 3 sensors, and i...

KSZ8863 RMII Interface and STM32f207 Communication

Posted on November 09, 2017 at 20:22Hello,I am currently using HAL library to interface my STM32F207 to a KSZ8863 switch using RMII Interface. The clock 25 Mhz provided externally which is then scaled to 50 Mhz to enable the interface. Now, I can re...

R B by Associate
  • 1821 Views
  • 1 replies
  • 0 kudos

Error handling for UART RX with DMA

Posted on January 15, 2018 at 11:00Hello!I am using RX DMA with RX timeout detection (based on Efficiently receive UART data using DMA). Under normal condition, everything works fine, but I have problems with the error handing. My MCU is the F302R8 ...

0690X00000604D4QAI.jpg
T B by Associate II
  • 1358 Views
  • 1 replies
  • 0 kudos

Adding TIM7 (timer 7) with interrupt using STM32CubeMX

I tried to add TIM7 via CubeMX with interrupt on NUCLEO-H743ZI.CubeMX was able to create the init for the timer in the code but it didn't add the IRQ, didn't enable the IRQ and didn't add its callback.I added this code manualy.What I'm missing?

Yood by Associate II
  • 637 Views
  • 1 replies
  • 0 kudos

Waking up STM32L0 from LPTIM interrupt

Posted on July 13, 2018 at 03:12I'm trying to put STM32L0 into a low power sleep mode. I want it to sleep for 9.5s and wake up for 0.5s. Once it's awake it needs to switch on LEDs, check for any interrupts from a Lora radio module and process the da...

Ash G by Associate II
  • 1553 Views
  • 1 replies
  • 0 kudos