2018-12-16 04:17 AM
Hello.
I have a nucleo powered with external 5V. I use to log info using usb.
Eache time i need to talke a log to the log, i cannoct my laptop and MCU reset.
Anyone know if i can hovoid this? Remove SB12 could help Me? any other hint?
Regards,
Carmelo
2018-12-16 06:53 AM
What version of ST-LINK firmware is being used on the board?
The reset pin may also have a solder bridge which you could remove.
2018-12-16 07:34 AM
thanks,
Version is :
16:32:15 : ST-LINK Firmware version : V2J28M17
i Try check on schematics but theonly sb o foun on NRST is sb12. I0m not shure it the rigth one.
2018-12-16 10:12 AM
I don't have the schematic to hand.
The STM32 will reset itself if the VDDA supply glitches or browns-out.
2018-12-16 10:21 AM
Disconnect the SWD jumpers on CN2.
When you'll want to program connect them back.
JW
2018-12-17 05:52 AM
hello, unfortunatly doesnt work.
carmelo