2025-03-04 9:08 PM
I am using STM32s NUCLEO-H755ZIQ board , while debugging through eclipse IDE for the M7 core the board's MCU went under low power state and LD6 which is over current led (red) is turned on.
When I am connecting the board with the STM32CubeProgrammer the board is gettting detected but ST-Link is failing to flash the board.
Please help me with this problem as same thing has happend with the another NUCLEO-H755ZIQ board.
Both the boards are having same problem
Solved! Go to Solution.
2025-03-05 2:46 AM - edited 2025-03-05 3:01 AM
In that case either:
1- This regulator is internally short-circuited :
2 - Or you have a short circuit on the board.
To differentiate between the two cases you need to unsolder SB2 and fit again JP2.
If LD6 is lit: the regulator is broken. You need to purchase another board.
If LD6 is off you have a short circuit on the board. In that case you need to check your board and find if VDD is short-circuited.
Hope that helps.
2025-03-04 11:29 PM
Hello @Shubhamkeshari and welcome to the community,
@Shubhamkeshari wrote:
while debugging through eclipse IDE for the M7 core the board's MCU went under low power state
How do you know it's a low power mode?
What example are you using?
Did you generate the project with CubeMx? if yes, Are you using STM32CubeIDE?
2025-03-04 11:36 PM
The project I have flashed is developed on Zephyr RTOS.
Which has multiple threads 5 in working at a time.
This is the message comming when I am connecting with STM32CubeProgrammer
2025-03-04 11:47 PM
The voltage is very low: 0.87:
Check the VDD voltage level with a multimeter on JP4.
2025-03-04 11:49 PM
Yes , it is comming 0.433V
Is my board short ?
2025-03-04 11:55 PM - edited 2025-03-04 11:55 PM
What is the position of the jumper here?:
And how are you powering the board? via ST-Link?
2025-03-05 12:21 AM
The position of the jumper is same as the image.
The board is been powered by a USB cable
I have changed the USB cable and tried, still the same
2025-03-05 12:33 AM
USB cable connected to CN1 (ST link USB connector)?:
2025-03-05 12:35 AM
Yes, I have connected in that USB port
2025-03-05 12:54 AM
Ok,
1- Then, check if you have 5V on JP2 on one of these pins:
LD5 is On?
2- After, check if you have 3.3V on SB2: