cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H755ZIQ MCU went under low power state while debugging

Shubhamkeshari
Associate

I am using STM32s NUCLEO-H755ZIQ board , while debugging through eclipse IDE for the M7 core the board's MCU went under low power state and LD6 which is over current led (red) is turned on.

When I am connecting the board with the STM32CubeProgrammer the board is gettting detected but ST-Link is failing to flash the board. 

 

Please help me with this problem as same thing has happend with the another NUCLEO-H755ZIQ board.

Both the boards are having same problem 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

In that case either:

1- This regulator is internally short-circuited :

mALLEm_0-1741171206855.png

2 - Or you have a short circuit on the board.

To differentiate between the two cases you need to unsolder SB2 and fit again JP2.

If LD6 is lit: the regulator is broken. You need to purchase another board.

If LD6 is off you have a short circuit on the board. In that case you need to check your board and find if VDD is short-circuited.

Hope that helps.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

20 REPLIES 20
mƎALLEm
ST Employee

Hello @Shubhamkeshari and welcome to the community,

 


@Shubhamkeshari wrote:

while debugging through eclipse IDE for the M7 core the board's MCU went under low power state


How do you know it's a low power mode?

What example are you using?

Did you generate the project with CubeMx? if yes, Are you using STM32CubeIDE?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The project I have flashed is developed on Zephyr RTOS.

Which has multiple threads 5 in working at a time.

 

Shubhamkeshari_0-1741160128729.png

This is the message comming when I am connecting with STM32CubeProgrammer

The voltage is very low: 0.87:

mALLEm_0-1741160743775.png

Check the VDD voltage level with a multimeter on JP4.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes , it is comming 0.433V 

Is my board short ?

mƎALLEm
ST Employee

What is the position of the jumper here?:

mALLEm_0-1741161321969.png

And how are you powering the board? via ST-Link?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The position of the jumper is same as the image.

The board is been powered by a USB cable 

I have changed the USB cable and tried, still the same 

USB cable connected to CN1 (ST link USB connector)?:

mALLEm_0-1741163562152.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes, I have connected in that USB port

Ok,

1- Then, check if you have 5V on JP2 on one of these pins:

mALLEm_0-1741164763873.png

LD5 is On?

2- After, check if you have 3.3V on SB2:

mALLEm_1-1741164807146.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.