cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H755ZIQ MCU went under low power state while debugging

Shubhamkeshari
Associate III

I am using STM32s NUCLEO-H755ZIQ board , while debugging through eclipse IDE for the M7 core the board's MCU went under low power state and LD6 which is over current led (red) is turned on.

When I am connecting the board with the STM32CubeProgrammer the board is gettting detected but ST-Link is failing to flash the board. 

 

Please help me with this problem as same thing has happend with the another NUCLEO-H755ZIQ board.

Both the boards are having same problem 

20 REPLIES 20

No, i dont have 5V and 3.3V on the pins 

No , i am not getting either 3.3V and 5V

Most probably that regulator was broken:

mALLEm_0-1741167191095.png

Check if you have 5V on R25 or C40 pads. If you get that voltage, this means (unfortunately) the regulator is broken. Need to have another board.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I got 0.98V on R25 and C40 pads

1- Are you sure you don't have 5V on the JP2?

 mALLEm_0-1741164763873.png

2 - LD5 is normally lit?

3 - Check the voltage on 5V_USB_STLK: the pad of the capacitor C1:

mALLEm_0-1741168806876.png

4 - LD6 is normally lit?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes i am sure that i don't have 5V on JP2

LD5 is very -very dim

Voltage at C1 is 1V

What about the voltage level on 5V_USB_CHRG (check R2 pad)? 

 LD6 is lit?:

mALLEm_0-1741170235300.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes this is lit

If LD6 is lit: you have an overcurrent on the board.

If you remove JP2:

mALLEm_0-1741164763873.png

LD6 still lit?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

When I remove JP2 LD6 is not lit