NUCLEO-H743ZI board LD39050PU33R
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-10 12:40 PM
On the NUCLEO-H743ZI board the LD39050PU33R 3.3 volt LDO provides voltage but what is the Vd or Vdrop for the LD39050PU33R?
I found I can add 3.7 volt (18650 battery) to JP3 pin 3 : I can't use VBAT as it is wired to 3.3 volts.
Object, run board on battery!
Thanks...
#nucleo-h743zi- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-10 1:32 PM
Data Sheet says 200mV
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-10 3:46 PM
I use this one, AP2114H-3.3TRG1, it is the same PNP type regulator, but will drive upto 1.4A ( probably only because it can remove the heat easier..)
dropout voltage under 0.2V at 400mA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-10 7:01 PM
I'm use to the .7 drop from years ago, after reading about the device I'm hooking to 'Supply voltage range: 3.0V~ 4.3V, Typ: 3.8V' I'm going to us a STM32L452 at 1.8 volt to control the CAT-M1 device (it's I/O is 1.8 V) with a solar powered Lipo at 3.7 volt. DigiKeys price was impressive at $399, a few more than needed... Mouser has 1 @ pricing, $0.36.
I'm waiting on a NUCLEO-L452RE-P I ordered yesterday for power testing.. The
NUCLEO-H743ZI
was using .18 amp and I expect the NUCLEO-L452RE-P to be around 10 times less or about .08 amp - without the ST-Link part the current will drop it more.