2025-09-22 3:33 AM
Hi,
I’m working with the NUCLEO-H723ZG board and would like to know if it’s possible to use its two DAC outputs to generate a differential signal.
Thank you very much
2025-09-22 3:52 AM
Don't really know, probably yes if you feed both DACs with DMA and sync them with a timer.
I'd prefer to do this on the analog side.
2025-09-22 5:33 AM
Yes, this is possible.
2025-09-22 8:17 AM
No. Fully Differential signals means two path are correlated. Having two dac's output 180 degree phase shifted sinewave generates two SE.
But you can easily synthesize diff by one dac and inverter.
2025-09-22 2:33 PM
Analog side this mean putting an external component? A differential amplifier for the example?
2025-09-22 2:33 PM
Thank you
Do you know how?
2025-09-22 4:07 PM
Have one channel be the positive side and another channel be the negative side. Set up a buffer for the values and set up a timer to trigger conversions so they stay in sync.
Two single ended signals that are coherent = differential signal. At least for the driving side.