cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-G431 onboard stlink can't work

lianglei001x
Associate

Nucleo-G431 onboard stlink used normally before, but recently it suddenly couldn't be used, there was no response when connected to the computer with a USB cable, the computer could not detect the stlink (it can be determined that there is no problem with the USB cable, there is no problem with the computer driver, and there is no problem with connecting other stlinks), the power supply of the test main control chip is normal, and the crystal oscillator vibrates normally, what is the reason for this, is there a solution?

3 REPLIES 3
Imen.D
ST Employee

Hello @lianglei001x ,

Try to upgrade your ST-Link firmware to the latest version and verify that all jumpers are correctly configured.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

lianglei001x_0-1726016720982.jpeg

Hello Imen.D,
I checked the jumper and it was the same as on the manual. Nucleo-G431 cannot be recognized by the computer, all the indicator LEDs are not lit after plugging in the computer via USB, and it cannot be connected to the stlink utility or stm32Cubeprogrammer, is there any other way to update the firmware?

 

 

Hello, use another cable and check

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.