cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo F401RE Virtual USART Crashing

ANels.1
Associate II

I currently have a project using micropython on the Nucleo F401RE. When connected to the virtual USART over usb, it seems to crash every 15min or so. I've tried connecting directly to PA2 and PA3 (while doing all the other setup to enable it) and it runs completely fine without crashing at all.

4 REPLIES 4

Dell? Disable Diagnostic Agent and Intel Tools

Got most current firmware on ST-LINK?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I am on a Dell, but I dont have the Diagnostic Agent nor the Intel tools (as far as i know, after looking through the system).

I've got the most current version of the ST-LINK also (V2.J34.M25), and i've done an update anyway to see if that fixes the problem, all to no avail.

Check registry for UpperFilters and LowerFilters​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Not there unfortunately, here's what i see when i open up the specific GUID class:

0693W000000WxZsQAK.png