2016-04-27 09:30 AM
Hi gang,
How do I set up Keil with this new dev board, including the ST-Link/V2-1?Cant see this board in thehttp://https://www.keil.com/boards2/
(as I guess is quite new). But actual is in the .I've installed the 'Device Family Pack', and so can now see the STM32F042K6 from within the 'Device Database'.Cheers #nucleo #keil2016-04-28 03:59 AM
Hi chendy,
Try to use the Pack Installer to install the Software Pack, or try to download and install the pack directly from this .-Syrine –2016-04-29 04:14 AM
I have done so, but what next to get a pin toggling etc?
Are there any guides for setting up a new project for a board that is currently unsupported (despite it being sold to me!)?thanks2016-04-29 06:23 AM
Hi chendy,
STM32Cube_FW_F0_V1.5.0\Projects\STM32F042K6-Nucleo\Examplesthis directory contains a set of examples based on STM32F042K6-Nucleo board, it will be very helpful as staring to develop your own application.-Syrine –2016-05-10 07:07 AM
Are there any examples for USB Serial?
2016-05-10 08:46 AM
Are there any examples for USB Serial?
Using the VCP provided by the Nucleo board, or running natively on the F042K6 ?