2025-01-15 4:23 AM - last edited on 2025-01-15 4:33 AM by Andrew Neil
Title edited: just "STM32CubeIDE" doesn't tell anything of what the post is actually about - especially in the STM32CubeIDE forum!
Hello Team,
I wanted to generate the code through the STM32CubeIDE and use the Keil simulator to test the code.
I have gone through this pdf https://www.keil.com/appnotes/files/apnt_323.pdf,
But when I try to do this same thing with the STM32H743BIT6 controller, I am not able to change the Toolchain.
Could you please help me with this?
2025-01-15 4:28 AM
Welcome @Akhilesh_30, to the community!
you have to use the stand-alone STM32CubeMX if you need to create code for other toolchains than CubeIDE.
Hope that helps?
Regards
/Peter @