cancel
Showing results for 
Search instead for 
Did you mean: 

Not entering to sleep mode immediatly after Programming STM32 controller using STlink programmer

darshan-ltts
Associate II

I am working with STM32 U575/U5A5 and L4 series of STM32 controllers in low power mode. I have programmed the controller to wake for every 10s and blink LED. This issue what we observed is once  immediately flashing hex file to controller using STlink programmer, Controller is not entering in sleep mode LED will be keep on blinking. If I remove the power and connect it back, Controller is entering sleep mode and waking up for every 10s as expected.

we have reseted the controller using Reset button, but still controller is not entering to sleep mode.

The question here is why Controller requires  power on reset to enter power saving mode after flashing hex file to controller using STlink programmer?

 

27 REPLIES 27

So the MCU does still behave the same as if went to sleep - you just don't get the power reduction.

So this doesn't explain why @darshan-ltts does see different behaviour.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil No... It won't go to sleep. Means If I configure wakeup for 10s, It'll wake up immediately and power consumption is also more. Problem is as per our product requirement, if main power is not available, Controller we are keeping in sleep mode and we are expecting the backup of 50Hrs and device is Potted., If we flash the firmware from the cube programmer, we need to keep for        3-4hrs to discharge and then need to test the functionality. 

Try place in your code reset DBG CR to zero. Or you in programmer activate RDP option bytes, this is next block require power off... And you still write about sleep mode , but real preserve is STOP mode.

BarryWhit
Lead II

@darshan-ltts , the real problem here is that none of us can be sure we understand what problem you're describing due to language barrier. Please make an effort to be as clear as possible.

 

My initial post suggested a very quick and concrete test for you to make, which would clarify things.  Have you done the test I described? what are the results?

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.

@darshan-ltts wrote:

It won't go to sleep. Means If I configure wakeup for 10s, It'll wake up immediately 


That doesn't really make sense - if it never goes to sleep, how can it ever wake up?

Again, have you tried this in the debugger to see  what's happening?

 


@darshan-ltts wrote:

and power consumption is also more. 


That is to expected - @MM..1  explained the reason.

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

If I do power cycle not button reset. Then I can see device wake up for every 10s

Again, have you tried this in the debugger to see  what's happening?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

no I haven't tried.. because it is not the usecase for us. Mainly issue is because of production 

BarryWhit
Lead II

I'm out.

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.

@darshan-ltts wrote:

no I haven't tried.. because it is not the usecase for us. Mainly issue is because of production 


What ??

Do you want to fix this problem?

If you want to fix it, you will need to find it first.

The purpose of using the debugger is to find the problem!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.