2017-04-07 2:22 AM
Hi,
I'm working with STM32F030k6 and I wrote simple custom boot loader which will jumps to application.
Below is custom boot loader code.
__disable_irq();
SCB->VTOR = go_address; //0x08000C00 // NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0C00); if (((*(__IO uint32_t*)go_address) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (go_address+ 4); JumpToApplication = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) go_address); JumpToApplication(); }Jumping to application is success but when I'm trying to send data over uart board is getting restart. Please help me if some one would have face this issue.