NOR Flash(external memory )- Status error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-16 3:11 AM - last edited on 2024-04-21 1:59 AM by Peter BENSCH
Hi all,
I'm working on the NOR Flash via OSPI(using as QSPI) with the STM32U585 board. implementing this via filex and levelx, i have done all the configuration referring to the example provided by ST with the minor changes. I'm getting error in the following part of code.
the status return for this should be success but its getting failed. even i tried in the same example one which provided by the ST for the U5 board, even their I'm getting the error.
could someone help me what could be the problem for getting failure return.
/* Format the OCTO-SPI NOR flash as FAT */
nor_ospi_status = fx_media_format(&nor_ospi_flash_disk, // nor_ospi_flash_disk pointer
fx_stm32_levelx_nor_driver, // Driver entry
(VOID *)LX_NOR_OSPI_DRIVER_ID, // Device info pointer
(UCHAR *) fx_nor_ospi_media_memory, // Media buffer pointer
sizeof(fx_nor_ospi_media_memory), // Media buffer size
FX_NOR_OSPI_VOLUME_NAME, // Volume Name
FX_NOR_OSPI_NUMBER_OF_FATS, // Number of FATs
32, // Directory Entries
FX_NOR_OSPI_HIDDEN_SECTORS, // Hidden sectors
(LX_STM32_OSPI_FLASH_SIZE - LX_STM32_OSPI_SECTOR_SIZE)/ FX_NOR_OSPI_SECTOR_SIZE,// Total sectors
FX_NOR_OSPI_SECTOR_SIZE, // Sector size
8, // Sectors per cluster
1, // Heads
1);
- Labels:
-
OctoSPI
-
STM32U5 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-25 8:01 AM - edited 2024-04-25 8:03 AM
Hello @meghasb ,
Which memory are you using?
Is it the same memory used in Fx_NoR_Write_Read_File example: MX25LM51245G?
Could you please check the OCTOSPI and the hardware configuration.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.