2020-08-06 03:42 AM
Hello community! I have a problem please help me out, I am trying to interface NFC05A1 with STM32F469 discovery board using the demo provided by ST for F4, L4. NFC05A1 is initializing and a message is sent to serial terminal "Welcome to X-NUCLEO-NFC05A1, RFAL initialization succeeded " but NFC05A1 is not reading any tag ,P2P and not even a Led blinks when field is close to it as there is no error in the program.
2020-08-06 08:09 AM
The problem is solved by calling the st25r3911Isr(); in EXTI0_IRQHandler() in stm32f3xx_it.c file.
Now another issue is that it is only reading the card once upon pressing the user button (executing only once) how to solve this.