cancel
Showing results for 
Search instead for 
Did you mean: 

New STM32F4xx Reference Manual RM0090

waclawek.jan
Super User
Posted on November 05, 2012 at 11:28

Revision 2 of RM0090 is available.

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REFERENCE_MANUAL/DM00031020.pdf

JW
This discussion is locked. Please start a new topic to ask your question.
29 REPLIES 29
waclawek.jan
Super User
Posted on June 12, 2013 at 18:11

STM32F405/407 datasheet is rev4 now.

waclawek.jan
Super User
Posted on February 12, 2014 at 14:57

RM0090 rev.6 is out.

Uwe Bonnes
Principal III
Posted on February 12, 2014 at 16:16

> RM0090 rev.6 is out.

Is there any chance that ST gets their document system a little more sane like:

- provide date of last release on the website.

- not to use 4 names for the same document.

Posted on February 12, 2014 at 18:45

The use of RM0090 has been pretty consistent. There are dozens of Data Sheet/Manuals for specific part designations.

The site is a bit of an unmanageable train wreck.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on February 12, 2014 at 19:00

>> - not to use 4 names for the same document.

> The use of RM0090 has been pretty consistent.

I believe Uwe meant the fact that for example RM0090 goes under the DM00031020.pdf filename, and is labelled on the pages' footer as Doc ID 018909. This is similar for the other published materials.

JW

waclawek.jan
Super User
Posted on May 23, 2014 at 17:24

RM0090 rev.7 is out.

waclawek.jan
Super User
Posted on December 01, 2014 at 09:41

RM0090 rev.8 is out.

waclawek.jan
Super User
Posted on March 30, 2015 at 12:38

RM0090 rev.9 is out.

waclawek.jan
Super User
Posted on August 13, 2015 at 12:29

RM0090 rev.10 is out.

waclawek.jan
Super User
Posted on October 29, 2015 at 18:12

RM0090 rev.11 is out.

Datasheet for STM32F40x is in it new rev.6 too. I did not check for other STM32F4xx, but I assume they have new revisions of datasheets too. An interesting detail, reflected both in the datasheet and RM0090 is that the allowed range for PLLs output is now extended downwards to 100MHz. Strangely, the datasheet states the same power consumption at this frequency as it used to be for the significantly higher 192MHz... Could somebody from ST comment on this, please?

JW