2016-08-01 7:54 PM
I just installed for the first time, I am familiar with eclipse, and when I attempted to create my first project I get the error
jconfig.h,No such file or directoryI have a stm32f7 disco board that I am trying to figure out. I downloaded the firmware but can't make any progress.edit:I found a version from the jpeg group that had jconfig.h so I used it, I have no idea if it resembles what I need? I then had the error jmorecfg.h missing and I found one of those, but it doesn't seem correct. Why, I don't know :)Because I have errors that don't make sense except if something is wrong.Description Resource Path Location Typeexpected '=', ',', ';', 'asm' or '__attribute__' before 'read_file' jinclude.h /ATest/Middlewares/Third_Party/LibJPEG/include line 93 C/C++ Problem #!stm322016-08-09 8:26 AM
Hi madigan.ray,
1- What do you need to do exactly with the STM32F7 discovery?2- Are you looking for an IDE? I recommend you to use the . 3- Do you need Eclipse in order to be able to use the MX plugin? If yes, please refer to resources available in .-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.