2022-07-21 12:20 AM
I was Displaying HSI on Serial Port using Alternate Functions, as soon i enabled the HSI i got the following error messege.
Target no device found
Reason: No device found on target.
Looking Forward for help.
Regards.
2022-07-21 2:27 AM
"Displaying HSI on Serial Port using Alternate Functions"
What do you mean by that?
"as soon i enabled the HSI i got the following error"
Do you mean
"Target no device found Reason: No device found on target."
Have you checked connections, power supplies, etc?
Did you change the code to go into a sleep mode, and/or disable the debug pins?