Moving from STM32L476xx to STM32L4R9xx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-30 5:05 PM
After spending some time looking into the R9 I decided to make the switch. I've been developing on the 76 for a while now. I read the migration document and it doesn't look like there are any differences.
Right now I'm having issues with spi and sd card / fatfs stuff. After several days of reading I really can't figure out what's goin on. I've changed the linker script, startup.s asm, and the define in the Makefile. I know the sdio driver uses an internal DMA, so I just pulled out the DMA stuff and linked up a callback... No dice. For the spi I changed the clock divider because I'm running the hclk faster (120)
I'll post some code tommorow but I have to be missing some major component...
- Labels:
-
DMA
-
SPI
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-30 5:40 PM
Looks like you've got DMA on SDMMC handled differently on L4+
CLOCKDIV math also different, and peripheral clock sourcing. So CLKCR and HSI/PLL sources
Perhaps check command line option/defines, and merge in example code from an L4+ BSP
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_PeriphCLKInitTypeDef RCC_PeriphClkInit;
/* Check whether HSI48 is enabled or not */
HAL_RCC_GetOscConfig(&RCC_OscInitStruct);
if(RCC_OscInitStruct.HSI48State != RCC_HSI48_ON)
{
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
while(1) {}
}
}
/* Configure the SDMMC1 clock source. The clock is derived from the HSI48 */
RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SDMMC1;
RCC_PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_HSI48;
if(HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphClkInit) != HAL_OK)
{
while(1) {}
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
2019-07-31 10:25 AM
I'm not using the HSI48, I routing through some PLLs to generate my clock for SDMMC1. Here is my clock code.
#ifndef __CLOCK_H
#define __CLOCK_H
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 60;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV5;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_SDMMC1
|RCC_PERIPHCLK_OSPI;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_PLLP;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
#endif /* __CLOCK_H*/
Here's my sd init
sd::sd(SD_HandleTypeDef &sdi)
:rsd(sdi),SDMounted(false), _error(false)
{
__HAL_RCC_SDMMC1_CLK_ENABLE();
__HAL_RCC_DMAMUX1_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct = {0};
rsd.Instance = SDMMC1;
rsd.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
rsd.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
rsd.Init.BusWide = SDMMC_BUS_WIDE_1B;
rsd.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
rsd.Init.ClockDiv = 64;
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDMMC1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDMMC1;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
HAL_SD_Init(&rsd);
HAL_SD_RegisterCallback(&rsd, HAL_SD_READ_DMA_DBL_BUF0_CPLT_CB_ID, &rxcb);
HAL_SD_RegisterCallback(&rsd, HAL_SD_WRITE_DMA_DBL_BUF0_CPLT_CB_ID, &txcb);
HAL_SD_RegisterCallback(&rsd, HAL_SD_READ_DMA_DBL_BUF1_CPLT_CB_ID, &rxcb);
HAL_SD_RegisterCallback(&rsd, HAL_SD_WRITE_DMA_DBL_BUF1_CPLT_CB_ID, &txcb);
//rsd.Read_DMADblBuf1CpltCallback(SD_HandleTypeDef*) = &txcb;
//rsd.Write_DMADblBuf1CpltCallback(SD_HandleTypeDef*) = &rxcb;
/* Enable the Global Interrupt*/
HAL_NVIC_SetPriority(SDMMC1_IRQn, 6, 1);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
mount(); //Mount the SD card.
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-31 11:07 AM
Alright I've gotten the spi working again by calling
__HAL_RCC_DMAMUX1_CLK_ENABLE();
Hopefully it's something similar to this with the sd card stuff