2013-08-06 08:10 AM
#define USART_WordLength_8b ((uint16_t)0x0000)
#define USART_WordLength_9b ((uint16_t)0x1000) hello forum,I am trying to modbus ascii comunicate with a delta operator panel the settings of OPanel is 7 bit data, 1 stop, 1 parity however my STM32F103 has only the above settings why there is no 7 bit wordlength ? what can I do else ?thanks #modbus-ascii-stm32f1032013-08-06 08:15 AM
7-bit + 1-bit (parity odd or even) = 8-bit
You program the STM32 as 8-bit, and enable parity. This will enable 7N1 or 7O1 in the classic sense. For 8N1 or 8O1 you'd configure in 9-bit mode.2013-08-12 11:23 AM
hello ,
I did what you said ; I setup serial port 7Even1 ( 8 bit word length + even parity ) what I want is to connect my STM32F103 to Delta HMI operator panel with modbus ascii when I request some internal memory of HMI , it responds with an ascii array just like modbus standart says as you know modbus ascii has terminating characters 0xd 0xa however when I watch the received ( by the STM32 ) characters I see 0x8d and 0xa how can a serial port receive an 8 bit character with 7E1 setup ? thank you PS. delta HMI is also setup 7 E 12013-08-12 12:18 PM
That should have been 7E1 and 8E1 above.
You'll want to mask the data from USARTx->DR to remove the parity bit. Basically USART_ReceiveData(USART1) & 0x7F; for the 7-bit case and USART_ReceiveData(USART1) & 0xFF; for the 8-bit case. The register is 9-bits long.2014-11-11 09:15 AM
I am trying to get 8E1 to work right now I get 7E1 , I have a board with
32bit STM32F427 Cortex M4
and I using the operation system to open the Uart etc, how do I set theUSART_WordLength_9b to make the STM send 8E1
Itay2014-11-11 09:58 AM
I am trying to get 8E1 to work right now I get 7E1 , I have a board with 32bit STM32F427 Cortex M4 and I using the operation system to open the Uart etc, how do I set the USART_WordLength_9b to make the STM send 8E1
Itay
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* Enable USART1 Clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1); /* Connect PB6 to USART1_Tx*/
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1); /* Connect PB7 to USART1_Rx*/
/* Configure USART1 Tx & Rx as alternate function */
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_9b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_Even;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure); /* Configure USART */
USART_Cmd(UART1, ENABLE); /* Enable the USART */