Question
Ulink2
Posted on November 08, 2014 at 21:27 IDE: Keil 4.74 (microvision) Board: proprietary board with STM32F102C8 Program: only activates UART 1 to communicate with a terminal 1 - I can download the program to the board using the Flash Loader Demonstrator, the program works fine 2 - IDE debug mode: the Ulink2 is detected but: ''Ulink2 communication failure'' 3 - This same Ulink2 works perfectly on another board with STM32F103VB and exactly the same program. 4 - The JTAG pins are routed the same way on both boards. I checked them with an auxiliary program disabling the JTAG and outputting a 1Mhz square wave at these pins, one by one. Any clue? Could it be that the Jlink2 doesn't support the STM32F102 anymore?