cancel
Showing results for 
Search instead for 
Did you mean: 

mmc deinit problem

cgamu
Associate

Hi,

We are working on a low power application which uses an emmc memory. Now we have problem when Deinit mmc driver. When mmc is disabled we have a base consumption of XXuA (stop 2 power mode) but when it is needed mmc must be enabled (using Init functions from HAL) and then disabled again (using DeInit functions from HAL). after this process it is not possible to reach again XXuA, a 8mA are added to the base consumption. Is it needed to add some deinit function to the system or must we disable (forced) some clocks or internal supplies to asure de-initialization of mmc driver?

 

Thanks

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @cgamu, to the community!

It would help potential helpers a little, if you could provide a few general conditions:

  • which MPU or MCU are you working with
  • what supply voltage does this device work with
  • what does your programme look like with which you switch the EMMC on and off

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Peter BENSCH ,

Thanks for your suggestions.

MCU: STM32U585VIT6

eMMC: ASFC4G31M-51BIN

Supply: 3V

Lines connected to uC:

cgamu_0-1724055708705.png

CODE:

static RetVal_t SDMMC1_MMC_Init(void) { RetVal_t result = IDN_OK; hmmc1.Instance = SDMMC1; hmmc1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING; hmmc1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE; hmmc1.Init.BusWide = SDMMC_BUS_WIDE_8B; hmmc1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE; hmmc1.Init.ClockDiv = 2; if (HAL_MMC_Init(&hmmc1) != HAL_OK) { HAL_MMC_DeInit(&hmmc1); result = ERROR; initialized = FALSE; } else { initialized = TRUE; } return result; } RetVal_t SD_hm_init(void) { RetVal_t result = OK; hal_gpio_request_info_t gpio_info; gpio_info.port = PWR_FLASH_EN_Port; gpio_info.pin = PWR_FLASH_EN_Pin; gpio_info.mode = GPIO_MODE_OUTPUT_PP; gpio_info.pull = GPIO_NOPULL; GPIO_Request(&gpio_info); GPIO_WritePin(PWR_FLASH_EN_Port, PWR_FLASH_EN_Pin, GPIO_SET); if (SDMMC1_MMC_Init() != OK) { result = ERROR; } else { } HAL_MMC_CardInfoTypeDef mmc_info; HAL_MMC_GetCardInfo(&hmmc1, &mmc_info); sdmmc_info.BlockSize = mmc_info.BlockSize; sdmmc_info.NumBlocks = mmc_info.BlockNbr; return result; } RetVal_t SD_hm_deInit(void) { RetVal_t result = OK; HAL_MMC_DeInit(&hmmc1); HAL_GPIO_WritePin(PWR_FLASH_EN_Port, PWR_FLASH_EN_Pin, GPIO_RESET); HAL_GPIO_Release(PWR_FLASH_EN_Port, PWR_FLASH_EN_Pin); return result; }
View more

Hope this helps,