2024-07-28 12:15 AM
Hi, I'm developing a STM32H750VBT6 board that need SDRAM, the datasheet said that only LQFP144 package does not support SDRAM, but I cannot find SDRAM option in FMC configuration. Can someone please help me.
2024-07-28 12:52 AM - edited 2024-07-28 12:53 AM
Hi,
(i never tried before...but) here on H750V ,
seems little bit "hidden" , only bank2 can be sdram :
2024-07-28 12:54 AM
I'd be surprised that the 100 pin part exports all the pins needed for SDRAM and the 144 pin doesn't.
Go through the pin table in the Data Sheet and check manually.