2025-06-19 4:22 PM
I am trying to write a single byte of data to the start of the EDATA area on the H533
I have the EDATA Sector 1 set to active via the option bytes.
static FLASH_EraseInitTypeDef EraseInitStruct;
uint32_t flash_sector_error;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.Sector = 24;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.NbSectors =1;
HAL_FLASH_Unlock();
if (HAL_FLASHEx_Erase(&EraseInitStruct, &flash_sector_error) != HAL_OK){
SEND_STRING("FLASH ERASE FAIL\r\n");
}
//HARDFAULT OCCURS HERE |V|
if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD_EDATA, 0x08030000, (uint32_t ) 43210) != HAL_OK){
SEND_STRING("FLASH WRITE FAIL\r\n");
}
HAL_FLASH_Lock();From my understanding in the reference manual the EDATA starts at 8030000 and is in sector 24 of bank 1.
The erase option works fine, but the HAL_FLASH_Program operation always causes a hard fault.
Suggestions? Next Steps for debugging?
Solved! Go to Solution.
2025-06-26 9:58 AM
I think I found the missing secret here.
I was missing the HAL_FLASH_OB_Launch(); call which sets the Option Start bit.
//configure option bits
HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct);
HAL_FLASH_OB_Launch(); //set the OPTSTART bit in OPTCR
2025-06-20 2:04 AM
Hello @TG_APCD,
If you read a flash high-cycle data not previously written, a double ECC error is reported and only a word full of set bits is returned. The ECC correction reports a double-error detection (ECCD) and ECCD implies an NMI raised.
Check this article: How to avoid a HardFault when ICACHE is enabled on the STM32H5 series
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-20 10:59 AM
Thanks, I'm not reading the region, I am erasing and then programming it.
I read through the linked article, and based on that I went and checked all the FLASH error registers to see if there were any flags raised following the fault.
I checked the NSCR, SECCR, NSSR, and the ECCDETR registers and didn't see any error flags raised there.
This is the state of the FLASH registers immediately following the hard fault.
ACR 0x1
NSKEYR 0x0
SECKEYR 0x0
OPTKEYR 0x0
NSOBKKEYR 0x0
SECOBKKEYR 0x0
OPSR 0x0
OPTCR 0x1
NSSR 0x0
SECSR 0x0
NSCR 0x602
SECCR 0x0
NSCCR 0x0
SECCCR 0x0
PRIVCFGR 0x0
NSOBKCFGR 0x1ff0001
SECOBKCFGR 0x0
HDPEXTR 0x0
OPTSR_CUR 0x2d30edf8
OPTSR_PRG 0x2d30edf8
NSEPOCHR_CUR 0x1
NSEPOCHR_PRG 0x0
SECEPOCHR_CUR 0x1
SECEPOCHR_PRG 0x0
OPTSR2_CUR 0xc300015c
OPTSR2_PRG 0xc300015c
NSBOOTR_CUR 0x80000c3
NSBOOTR_PRG 0x80000c3
SECBOOTR_CUR 0x0
SECBOOTR_PRG 0x0
OTPBLR_CUR 0x0
OTPBLR_PRG 0x0
SECBB1R1 0x0
PRIVBB1R1 0x0
SECWM1R_CUR 0x7
SECWM1R_PRG 0x0
WRP1R_CUR 0xff
WRP1R_PRG 0xff
EDATA1R_CUR 0x0
EDATA1R_PRG 0x8000
HDP1R_CUR 0x1
HDP1R_PRG 0x1
ECCCORR 0x0
ECCDETR 0x0
ECCDR 0x0
SECBB2R1 0x0
PRIVBB2R1 0x0
SECWM2R_CUR 0x7
SECWM2R_PRG 0x0
WRP2R_CUR 0xff
WRP2R_PRG 0xff
EDATA2R_CUR 0x0
EDATA2R_PRG 0x0
HDP2R_CUR 0x1
HDP2R_PRG 0x1 Also I realized there was another mistake in the code. I was not passing the pointer to the value to be written but the value itself, which I have fixed.
But that has not resolved the hard fault.
See the updated code below:
static FLASH_EraseInitTypeDef EraseInitStruct;
uint32_t flash_sector_error;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.Sector = 24;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.NbSectors =1;
uint32_t data_to_be_written =43210;
if(HAL_FLASH_Unlock()==HAL_OK)
{
SEND_STRING("FLASH UNLOCKED\r\n");
}
if (HAL_FLASHEx_Erase(&EraseInitStruct, &flash_sector_error) != HAL_OK){
SEND_STRING("FLASH ERASE FAIL\r\n");
}
else
{
SEND_STRING("FLASH ERASE OK\r\n");
}
//HARDFAULT OCCURS HERE |V|
if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD_EDATA, FLASH_ADDR, (uint32_t *)data_to_be_written) != HAL_OK){
SEND_STRING("FLASH WRITE FAIL\r\n");
}
else
{
SEND_STRING("FLASH WRITE OK\r\n");
}
HAL_FLASH_Lock();
Also for reference I am not using the ICACHE.
2025-06-26 9:58 AM
I think I found the missing secret here.
I was missing the HAL_FLASH_OB_Launch(); call which sets the Option Start bit.
//configure option bits
HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct);
HAL_FLASH_OB_Launch(); //set the OPTSTART bit in OPTCR