2018-03-09 11:06 PM
Hi, I've got a question related to making shields for Nucleo boards. The problem is portability of shields between boards. There are two questions, to which I can't find a simple answer:
1. Do ST Morpho connectors on various Nucleo-64 boards (with uCs in LQFP-64 package) share same pinout? Especially power and communications?
2. Is Morpho connector on new Nucleo-144 boards compatible with old Nucleo-64 boards? Of course, it's longer, but can I plug a shield on topmost part of the pin rows and expect it to work?
I tried looking at datasheets, but I'd have to compare multiple documents (schematics of Nucleo boards and datasheets of their uCs), so I think that if someone already researched this problem, it will be easier to just hear two boolean answers.
#nucleo-64 #nucleo-144 #stm32-nucleo-64 #st-morpho2018-03-10 1:54 AM
Well, the whole point of the Nucleo 'ecosystem' is precisely that common shields fit the whole range:
Sharing the same connectors, STM32 Nucleo boards can easily be extended with a large number of specialized application hardware add-ons (Nucleo-64 include Arduino Uno rev3 & ST morpho connectors, Nucleo-32 include Arduino Nano connectors).
http://www.st.com/en/evaluation-tools/stm32-mcu-nucleo.html?querycriteria=productId=LN1847
Click 'Resources' on that page --> Technical Literature --> User Manual
UM1956 User manual STM32 Nucleo-32 board
UM1724 User manual STM32 Nucleo-64 boards
UM2206 User manual STM32 Nucleo-64-P boards
UM2179 User manual STM32 Nucleo-144 boards
UM1974 User manual STM32 Nucleo-144 boards
So there is one User Manual for each series (except 144?!)
They give schematics & pinouts.
2018-03-10 3:03 AM
So there is one User Manual for each series (except 144?!)
See: