2021-03-15 02:23 AM
Hi Everyone, I am using STM32H757I-EVAL board and the onboard Twin Quad SPI Nor Flash ( MT25QL512ABB8ESF-0SIT ). I have configured QSPI to operate in DUAL Flash mode.
I am able to perform memory read, memory write, memory erase, and internal configuration register read operation from/to QSPI flash.
But, When I try to update NonVolatile configuration register, It fails to update it.
If I change my QSPI memory configuration from Dual Flash mode to Singal flash mode, It works for Flash-1.
So, Is there anything that I am missing for the Dual Flash Mode?
I am enabling Write Latch before write Operation.
As per the technical notes for STM32H757i_EVAL board, both flash needs to have an ideal configuration.
Here is the code snippet
int32_t WriteNonVolatileConfigurationRegister( QSPI_HandleTypeDef *Ctx, Interface_t Mode, uint8_t *pData )
{
QSPI_CommandTypeDef s_command;
/* Initialize the command */
s_command.InstructionMode = QSPI_INSTRUCTION_4_LINES;
s_command.Instruction = WRITE_NONVOL_CFG_REG_CMD; // 0xB1
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.DataMode = QSPI_DATA_4_LINES;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DummyCycles = 0;
s_command.NbData = 4; // QSPI_DUALFLASH_ENABLE = 0x04, QSPI_DUALFLASH_DISABLE = 0x02
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
/*write enable */
if( WriteEnable(Ctx, QPI_MODE)!= OK)
{
return ERROR_COMMAND;
}
/* Send the command */
if (HAL_QSPI_Command(Ctx, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return ERROR_COMMAND;
}
if (HAL_QSPI_Transmit( Ctx, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return ERROR_TRANSMIT;
}
/* Configure automatic polling mode to wait the memory is ready */
if( AutoPollingMemReady(Ctx, QPI_MODE)!= OK)
{
return ERROR_COMMAND;
}
return OK;
}
Solved! Go to Solution.
2021-03-15 07:13 AM
What Data? solved my issue!!!!
Expected Data is: { 0xF6, 0xF6, 0xFF, 0xFF }
Can write NonVolatile Config register !!
Thanks for your Question 🙂
2021-03-15 05:43 AM
And how's this called? What data? Does it wait on both devices? Does the Write Enable get to both?
2021-03-15 06:40 AM
Hi @Community member , Thanks for looking into this issue.
Does the Write Enable get to both?
-> Yes, The WriteEnable will set Write enable latch on both devices.
Does it wait on both devices?
->Yes, The AutoPollingMemReady will poll Write in progress bit from Flag Status register on both devices.
What data?
-> NonVolatile Configuration register is a 2Byte register, and I want 0 and 3rd bit to be zero ( default all bits are set to 1). So my data buffer is { 0xF6, 0xFF, 0xF6, 0xFF }
"The WRITE NONVOLATILE CONFIGURATION REGISTER operation must have input data starting from the least significant byte."
And how's this called?
-> This will be called by main.
WriteNonVolatileConfigurationRegister( &hqspi, QPI_MODE, nonVolatileConfigurationRegBuf );
uint8_t nonVolatileConfigurationRegBuf[4] = { 0xF6, 0xFF, 0xF6, 0xFF };
2021-03-15 07:13 AM
What Data? solved my issue!!!!
Expected Data is: { 0xF6, 0xF6, 0xFF, 0xFF }
Can write NonVolatile Config register !!
Thanks for your Question 🙂
2021-03-15 07:24 AM
Yes, data should be interleaved